Sigma - What port numbers are used by the Sigma system?

Issue

What Port numbers are used by the Sigma system?

Product Line

Satchwell Sigma

Environment

Ethernet communications

Ports

Port

TCP

UDP

Cause

What port numbers should be set as exemptions in the system firewall?

Resolution

Sigma server to Sigma NNN / controller communications - User Datagram Protocol (UDP)  uses port 49152.

Sigma server to Sigma client communications - Transmission Control Protocol (TCP) uses ports 3614 and 8080.

Sigma Web client communications - Transmission Control Protocol (TCP) uses ports 80 and 8080, but also uses port 3614.