Differences in packing material used on V241/V341 connection kits

Issue

There are 2 different packing types available for ordering when choosing connections for the V241/V341

Product Line

Field Devices

Environment

V241

V341

Cause

There is a difference in material used in the gaskets included with the connection packages.

Resolution

The "Packing, std" is a standard type gasket.

"Packing, spec" is intended to be used in primary circuit district heating applications. Material in gasket is PTFE.