Issue
How to set up Automatic DCU Save
Environment
All versions of I/Net Seven.
Cause
Setting up Automatic DCU Save and it does not work.
Resolution
To resolve this issue the following steps needs to be followed:
1. Go to Edit/Host Computer/Network Functions
2. Select the link that the controllers need to be saved on
3. Click on Setup and check the box to enable Daylight Savings Time
4. Put in the parameters 3-2-1 and 11-1-1 and click Okay.