Issue
Trend chart settings aren't saved. The properties dialogue is opened by right-clicking on the open trend chart and then one or more of the settings are changed. After that OK is pressed and then the chart is saved using the save button.
Product Line
TAC Vista
Environment
TAC Vista 5.1.7.
Cause
It appears that the new settings aren't being saved, but by clicking the save button before refreshing the trend chart the current "view" is saved - not the new settings entered in the properties dialogue.
Resolution
- Change the settings as described
- Click OK when finished with the settings
- Refresh the trend chart immediately
- Save it. The view with the new settings will be saved.
Another option in Windows 7:
- Right click on the chart object.
- Go to the "general" tab
- Uncheck Autoscale
- Enter the desired value.