Issue
When expanding the folders of a Niagara R2 station in Workplace Pro, a pop-up error appears: "cannot initialize view./tridium/props/error.properties#error E_invalid_enum_ordinal(6)".
After re-opening the station, the same error occurs. After rebooting the station, the error remains when the same folders are accessed.
Environment
Niagara R2 all versions
Cause
There is a revision difference between the jar files installed in the UNC and the jar files installed on the host computer.
Resolution
Identify which jar file versions are different and correct. More current jar files for all versions of Niagara R2 are available on The Exchange Download Center.