Issue
In the 'Make/Edit Badge' dialog of the personnel manager/editor, selecting 'Capture Photo' but nothing happens.
USB camera device works fine from an application other than Continuum.
Environment
CyberStation
Cause
The photo image source has not been properly selected.
Resolution
In the 'Tools' menu select 'Set Photo Image Source' menu item then select the camera device and click OK.
Clicking the 'Capture Photo' button works once the camera has been selected as the source.