Issue
Immediately after conversion from 9900 to 9680 an attempt to edit a system variable from the Continuum Explorer causes an access denied error
Environment
CyberStation
CX9680
Cause
Conversion process was not completely successful
Resolution
In the Continuum Explorer change the controller type to 9681, when the warning comes up that this is irreversible click OK
Change the controller type backup to 9680, when the warning comes up that this is irreversible click OK