Issue
Can two (or more) OPC servers be configured to get information from the same Continuum system?
Environment
CyberStation
OPC Server
Infinity CX controller.
Cause
General configuration
Resolution
Yes, multiple OPC servers can be configured to get information from the same Continuum system.
It is recommended that each OPC server runs in its own computer and uses a different CX as its primary controller.