Issue
What can be displayed in an OP7?
Can signals from programmable Xenta (Xenta 401, Xenta 301, Xenta 302, Xenta 281, Xenta 282, Xenta 283) be monitored/changed from OP7?
Environment
TAC Xenta Server (Xenta 701, Xenta 711, Xenta 721, Xenta 731)
TAC Xbuilder
TAC Xenta 401, Xenta 301, Xenta 302, Xenta 281, Xenta 282, Xenta 283
Cause
This is a way to display values from a Xenta server without using a PC
Resolution
The OP Tree contains all possible pages (not Graphics) and values that can be generated from the Xenta 700 web pages:
• Values pages
• Alarm pages
• Time Object pages
• Trend Log pages
• Variables
• System variables
• I/O signals
Any type of signal that can be displayed on either off these pages can be displayed in OP7