BACnet multi state object number of states and states label

Issue

Can the user set the 'Number of States' and the 'State Text' in a multi state object?

Product Line

Andover Continuum

Environment

CyberStation

bCX4040

All b3s

Cause

Function as designed.

Resolution

Continuum DOES NOT allow changes to the default number of states and state labels.

The 'Number of States' field is read only.

An attempt to change any of the label will result in the following error:

An error code was returned from a BACnet operation, but the reason could not be determined.