TAC Vista license version types required when upgrading.

Issue

Knowing which License to purchase when upgrading various scenarios.

Product Line

TAC Vista

Environment

TAC Vista License

Cause

Upgrade licenses are only available when a previous installation of Vista existed.

Resolution

When performing a major version upgrade to a Vista site, a new or upgrade license will need to be purchased depending on the scenario. While minor version upgrades are free. See below.

  • For major revision changes, for example from 4.x.x to 5.x.x, Upgrade Licenses cannot be purchased. Need to purchase "Brand NEW" Vista Licenses.
  • For minor revision changes, for example from 5.0.x to 5.1.x, Upgrade Licenses can be purchased.
  • For minor updates, for example from 5.1.x to 5.1.8 no license upgrades are required.

Note: When an upgrade license is used it can only be used for the same license type. An  example that is not available would be upgrading a Vista 5.0.x Standalone to a Vista 5.1.8 Manager license. The only upgrade license for this option would be Vista Standalone 5.0.x to Vista Standalone 5.1.8

Part numbers can be found in the Vista License Packages document.