Issue
How to transfer values between Menta object within the same Xbuilder project
Environment
TAC Xbuilder
Cause
Sometimes there is a need to transfer values between Menta applications in the same Xbuilder. To do this you create an input in the receiving node.
Resolution
- In Xbuilder open the Menta application that you want to read a signal from another Menta application
- Add a input block of the type the signal will be (II, RI or BI) save to Xbuilder.
- Right click on the input in the system pane and select "select signal"
- Browse to the signal you want to transfer.