Issue
Is there a easy way to manage Vista user accounts in many TAC Vista servers at same time?
Product Line
TAC Vista
Environment
TAC Vista 5.1.7
Cause
A user is a global object so if the Vista servers is in the same Vista network they should all have the same users.
If adding or deleting a user in one Vista server the user will be added or deleted in all Vista servers.
Resolution
Connect the Vista servers in a Vista server network.