Issue
Attempting to start I/A Series G3 Workbench generates the following error:
Exception in thread "main" java.lang.NoClassDefFoundError: com/tridium/sys/Nre
Caused by: java.lang.ClassNotFoundException: com.tridium.sys.Nre
at java.net.URLClassLoader$1.run(Unknown Source)
at java.security.AccessController.doPrivileged(Native Method)
at java.net.URLClassLoader.findClass(Unknown Source)
at java.lang.ClassLoader.loadClass(Unknown Source)
at sun.misc.Launcher$AppClassLoader.loadClass(Unknown Source)
at java.lang.ClassLoader.loadClass(Unknown Source)
at java.lang.ClassLoader.loadClassInternal(Unknown Source)
Environment
I/A Series G3 Workbench (all versions)
Cause
The software is unable to locate class files provided within the baja.jar file. The baja.jar is missing from the Niagara G3 module folder.
Resolution
Re-install Niagara and verify the path for installation is correct. If this does not correct the issue, manually copy all files from the I/A Series G3 installation CD module folder into the appropriate modules folder on the target computer.