Issue
Wants to run old UNC-600 station as an enterprise server but the license does not include LON. How do you order it?
Environment
I/A Series R2 Enterprise Server
I/A Series SoftJace
Cause
Customer wants to migrate a UNC-600 station to an enterprise server. The UNC-600 was already providing the needed database services so the station cannot be directly moved to a UNC. Even without the database service, the station may be too large for one UNC-520.
Resolution
Tridium does not make the LonWorks license available for the Enterprise Server or for the SoftJace.