Why doesn't the Known Occupancy Count number increase when Personnel enter the Area.

Issue

Why doesn't the Known Occupancy Count ( KnownOccupCount ) number increase when Personnel enter the Area.

Product Line

Andover Continuum

Environment

Continuum Access Control

Continuum Cyberstation

Cause

The Known Occupancy Count shows the current number of personnel in the given Area. The doors within that Area must have both Entry and Exit readers for this number to be incremented when people enter and decremented when people exit.

Resolution

The Known Occupancy Count will not function with Entry only doors. Both Entry and Exit readers are required on the doors within the Area.