Issue
The V395-1 is obsolete and no longer available
Environment
V395:
7319501000
7319505000
7319509000
7319513000
7319515000
7319519000
V321:
7312153010
7312157010
7312161010
7312165010
7312169010
TAC Forta
Cause
The V395 valve is obsolete and no spare parts or direct replacement valves are available.
Resolution
The closest suitable valve is the V321 with a Forta actuator. The "A to AB" measurements are the same, but the "A-AB centerline to B flange" is different. Double check the data sheets for more information and details.
Keep in mind that V395-1 is PN25, while the V321 is PN16.