Issue
How many LIPs can be used in Plug and Play mode when used in a Vista classic network
Environment
Loytec LIP's configured in plug and Play mode on a LNS network.
Cause
A limitation of 5 LIPs can be used on the Plug and Play mode on a single LNS network
Resolution
Select LIPs with the additional LON ports to allow your database to fit into 5 LIP limitation.
The options to enable a larger system than 5 LIPs are listed below:
- Use a network management tool like NL220 or LonMaker to configure the LIPs as routers.
- Purchase another NIC852 license and create another LNS network with a separate LIP as a config server.