Is the Personnel Import Utility (PIU) included with Continuum or is it add-on software?

Issue

Is the Personnel Import Utility (PIU) included with Continuum or is it add-on software?

Product Line

Andover Continuum

Environment

CyberStation

Cause

Documentation

Resolution

The Personnel Import Utility is part of the Continuum system but must be enabled in the CyberStation key before it can be used. The key must have the -D (Data Exchange) option in order for the PIU to work.

Note that the PIU is not to be confused with the Personnel Data Importer which is add-on software.