What are the different options on the CyberStation security key?

Issue

What are the different options on the CyberStation security key?

Product Line

Andover Continuum, Pelco Video Management

Environment

CyberStation

Cause

Documentation

Resolution

NOTE: These are the options used to program a security key but not necessarily what shows when a key is read using MMC key reader.

For example when a key is programmed for FIPS-201 it does NOT show the -F when the key information is read using MMC key reader, one way to know if FIPS-201 is enabled is to look at the Allowed Credentials setting in the Cyberstation, the FIPS credential options will be blank if the Cyberstation key is not enabled for FIPS-201

CyberStation:

SU-INT           Single User Integrated

SU-HVAC      Single User HVAC

SU-SEC        Single User Security

LAN-INT        LAN Integrated

LAN-HVAC   LAN HVAC

LAN-SEC      LAN Security

 

CyberStation Options:

-U                    Unlimited Points

-P                    Programmer’s Version

-B                    Badging Option

-CFRB1           Basic CFR Compliance Pack – 1st Workstation

-CFRBV1        Basic CFR Compliance Pack – 2nd Workstation & up

-CFRA1           Advanced CFR Compliance Pack – 1st Workstation

-CFRAV1        Advanced CFR Compliance Pack – 2nd Workstation & up

-D                    Data Exchange Option – includes Personnel Import Utility

-E2, 3                Endura integration option

-F1, 2                FIPS 201 option

-USB4             USB Key

 

1    Option requires special approval before it can be enabled.

2    Option only available through software upgrade process; cannot be ordered with new P/N configurations.

3    New option introduced in v1.91; required per workstation for integration with a Pelco Endura system. Currently this is free as of 8/2/14 but needs a cookie       from repair for this option to work

4    USB Key Option is mandatory for new orders

Note: The Continuum version number of a key, allows it to operate with all Cyberstation versions up to that release.