Issue
Does TreeTech version 3.1 & 3.2 support all block types in all types of GCMs and LCMs?
Product Line
TAC IA Series
Environment
- TreeTech version 3.1 or 3.2
- GCM-84xxx
- GCM-86xxx
- SIM-xxxxx
- LNC
- GIM-2100
- LCM-8xxxx
Cause
Block types supported are not listed in the Tree-Tech Engineering Guide document, F-26640
Resolution
The following table lists the sub-devices supported by TreeTech 3.1 or 3.2 for each Network 8000 device type.
GCM (rev 4.x & 5.x) | ASDGCM (rev 4.x & 5.x) | GIM-2100 / SIM-GCM (All rev) |
---|---|---|
LCM (rev 4.x) | LCM (rev 4.x) | MICROZONE-II |
LCM (rev. 5.x) | LCM (rev 5.x) | PEM |
MICROZONE-II | LIM | |
PEM | ||
LIM |
The following table lists the block types supported by each device family.
GCM 4.X | ASD-GCM 4.X | GCM 5.X | ASD-GCM 5.X | GIM-2100 | SIM-GCM | LCM 4.X/5.X |
---|---|---|---|---|---|---|
AI AIPLC ALARM AO AOPLC APT BTUH CALEN COS CURVE DAILY DCC DEGDA DELAY DI DIPLC DO DOPLC DPT EDL EMS ENTHL FLOW HILO HOLI LIMIT LOGIC LOOP MATH MOMEN MTR MZHP1 MZONE MZRT1 MZSAT MZST1 OSS POLL PULSE PWM RAMP RESET RLCM RNET SEQ SGCM SLECT SNET SYS TOTAL TREND TSTAT VVBOX WEEK |
ALARM AO APT BTUH CALEN COS CURVE DAILY DCC DEGDA DELAY DO DPT EDL EMS ENTHL FLO2 FLOW HILO HOLI LIM LIMIT LOGIC LOOP MATH MOMEN MTR OSS PEM1 POLL PWM RAMP RESET RLCM RNET SEQ SGCM SGRP SGRP2 SLECT SNET SYS TOTAL TREND TSTAT WEEK ZONE2 |
AI AIPLC ALARM AO AOPLC APT BTUH CALEN COS CURVE DAILY DCC DEGDA DELAY DI DIPLC DO DOPLC DPT EDL EMS ENTHL FLOW HILO HOLI LABEL LIMIT LOGIC LOOP MATH MOMEN MTR MZHP1 MZONE MZRT1 MZSAT MZST1 NIM NSCHD OSS POLL PULSE PWM RAMP RESET RLCM RNET SEQ SGCM SLECT SNET SYS TOTAL TREND TSTAT VVBOX WEEK |
ALARM AO APT BTUH CALEN COS CURVE DAILY DCC DEGDA DELAY DO DPT EDL EMS ENTHL FLO2 FLOW HILO HOLI LABEL LIM LIMIT LOGIC LOOP MATH MN MNFLO MOMEN MTR NIM NSCHD OSS PEM1 POLL PWM RAMP RESET RLCM RNET SEQ SGCM SGRP2 SLECT SNET SYS TOTAL TREND TSTAT WEEK Z2HSC Z2SCH ZONE2 |
ALARM AO APT BTUH CALEN COS CURVE DAILY DCC DEGDA DELAY DO DPT EDL EMS ENTHL FLO2 FLOW HILO HOLI LIM LIMIT LOGIC LOOP MATH MOMEN MTR OSS PEM1 POLL PWM RAMP RAV21 RDS21 RDV21 RESET RNET SEQ SGRP2 SLECT SNET SYS TOTAL TREND TSTAT WAV21 WDV21 WEEK ZONE2 |
ALARM AO APT BTUH CALEN CNTR1 CNTR2 COS CURVE DAILY DCC DEGDA DELAY DO DPT EDL EMS ENTHL FLO2 FLOW HILO HOLI LABEL LIM LIMIT LLLB1 LOGIC LOOP LWC1 MATH MN MNFLO MOMEN MTR NIM NSCHD OPM1 OSS PEM1 POLL PWM RAMP RECP1 RESET RMA1 RNET ROOF1 SEQ SGRP2 SIM SLECT SNET SYS TOTAL TREND TSTAT UNTV1 WEEK WMA1 WSHP1 Z2HSC Z2SCH ZONE2 |
AI ALARM AO APT BTUH CALEN COS CURVE DAILY DCC DEGDA DELAY DI DO DPT EDL EMS ENTHL FLOW HILO HOLI LABEL LIMIT LOGIC LOOP MATH MOMEN MTR NSCHD OSS POLL PULSE PWM RAMP RESET RGCM SEQ SLCM SLECT SYS TOTAL TREND TSTAT WEEK |
NOTE 1: Refer to the table at the beginning of chapter 4 of the GCM/LCM Programmer's Manual, F-23120, for more information on what object types are supported in specific versions or types of controllers.
NOTE 2: The block types listed for the "GIM-2100 / SIM-GCM:" encompass the blocks supported by all the devices of the group. You will be able to create any block type listed however, an error will be displayed when you attempt to download an unsupported block type into a specific controller in the GIM-2100 / SIM-GCM family. Please refer to the controller manual (LNC, SIM-York, SIM-Trane, SIM-CCN, SIM-MTech or GIM-2100) for information on the block types supported by that controller type.
The following ASD device blocks are supported by TreeTech.
MICROZONE II | PEM | LIM |
---|---|---|
AO DO EMS HOLI LOOP OSS RESET RGRP SCHED SEQ UI UTIL WINDO |
AO AS AT AV DI DO EMS LOOP RESET RGRP SEQ UTIL WINDO |
EMSA EMSD HOLI OVI RGRP RO SCHED UTIL WINDA WINDD |