Issue
The web service within the ENC-520 indicates a status fault - Unlicensed:javax.baja.license.FeatureNotLicensedException.
Environment
I/A Series G3, ENC-410, ENC-520
Cause
The web service has been added to the station however the ENC-520 is not licensed to support the web services. The web services status will indicate the fault condition and the ENC will not serve up graphics.
Resolution
Requires purchase of the web services option for the appropriate platform.
ENC-410-1 >> purchase ENC-410-WEB
ENC-520-2 >> purchase ENC-510-WEB