Issue
Error Codes:
Line | Level | Time Stamp | Error Code | TCB Addr | Prg Cntr | Data1 | Data2 |
1631 | E | 04/05/2012 10:55:30.00 | 0x0000640b | 0x04dd8500 | 0x02124e26 | 0x00005c20 | 0x00000000 |
Error Code Meaning: The Error Sys Var has been incremented
Line | Level | Time Stamp | Error Code | TCB Addr | Prg Cntr | Data1 | Data2 |
1632 | E | 04/05/2012 10:57:30.00 | 0x00001c0b | 0x04dd8500 | 0x02124e26 | 0x0000640b | 0x00000000 |
Error Code Meaning: GLB_ELOG_DUP_START
Product Line
Andover Continuum
Environment
Continuum Site with BCX Controllers and an Error Log
Cause
Crash of BCX and log reveals:
Line | Level | Time Stamp | Error Code | TCB Addr | Prg Cntr | Data1 | Data2 |
1629 | E | 04/05/2012 10:51:30.00 | 0x0000640b | 0x04dd8500 | 0x02124e26 | 0x00005c20 | 0x00000000 |
Error Code Meaning: The Error Sys Var has been incremented
Line | Level | Time Stamp | Error Code | TCB Addr | Prg Cntr | Data1 | Data2 |
1630 | E | 04/05/2012 10:53:30.00 | 0x0000640b | 0x04dd8500 | 0x02124e26 | 0x00005c20 | 0x00000000 |
Error Code Meaning: The Error Sys Var has been incremented
Line | Level | Time Stamp | Error Code | TCB Addr | Prg Cntr | Data1 | Data2 |
1631 | E | 04/05/2012 10:55:30.00 | 0x0000640b | 0x04dd8500 | 0x02124e26 | 0x00005c20 | 0x00000000 |
Error Code Meaning: The Error Sys Var has been incremented
Line | Level | Time Stamp | Error Code | TCB Addr | Prg Cntr | Data1 | Data2 |
1632 | E | 04/05/2012 10:57:30.00 | 0x00001c0b | 0x04dd8500 | 0x02124e26 | 0x0000640b | 0x00000000 |
Error Code Meaning: GLB_ELOG_DUP_START
Resolution
It is in the range of “Global System errors” that is usually not good, either faulty controller or need reloading of the O/S. Cold start and update O/S with the latest version supported by the Cyberstation version. Then run it on a test rig with different ID and see if it still crashes, if so will need to be repaired or replaced.