Forta actuator on valve V395

Issue

Is it possible to use the current Forta series actuator on the old V395 valve?

Product Line

Field Devices

Environment

V395:

7319501000
7319505000
7319509000
7319513000
7319515000
7319519000

TAC Forta

Cause

Forta application suitability.

Resolution

The Forta series actuators are suitable for use on the V395 valve. The data sheet for V395 has the M800 listed as recommended actuator.