Issue
Is the MNL-110 or MNL-130 controller available in any profile other than Fan Coil profile (F3)?
Environment
MNL controllers (MNL-110, MNL-130)
Cause
The MNL-110 and MNL-130 controllers are only available with the Fan Coil profile (F3). The profiles cannot be modified in the field.
Resolution
Review alternative hardware platforms (MNL-50, -100, -150, or -200) in the following profiles ...
- Rooftop profile (R3)
- Fan Coil profile (F3)
- Heat Pump profile (H3)
- Satellite profile (S3)
- Satellite profile (S4)