Continuum database fault warning events.

Issue

Continuum entries in the windows application events occasionally shows error related to the database connection.

A database fault warning state was detected and cleared. This is an
indication that the connection to the Continuum database was lost for a
moment.


"wuaueng.dll (46108) SUS20ClientDataStore: The database engine stopped
the instance (0)".

"wuaueng.dll (46108) SUS20ClientDataStore: The database engine started a
new instance (0)."


 

Product Line

Andover Continuum

Environment

CyberStation

Windows Event Viewer

SQL Server

Cause

Informational entries in the windows application event viewer frequently refer to Continuum reporting a database fault warning. The warning may or may not be accompanied with other information such as:

ClientDataStore: The database engine stopped the instance (0)

ClientDataStore: The database engine started a new instance (0)

These events can occur in the ordinary operation of the SQL Server environment, or they may be associated with errors.

Resolution

If a 'stopped' instance warning is immediately followed by a 'restarted' instance warning and not associated with an error then the event took place in the context of ordinary operation of the SQL server and can be ignored.

If on the other hand there is an error reported such as ‘The database instance ran out of disk space.’ then corrective action will be required.