Field Devices - SHR100 / SHR100 T combined temperature and humidity sensor connection details.

Issue

Unable to locate datasheet.

Product Line

Field Devices

Environment

SHR100

SHR100 T

Cause

Details of the temperature and humidity connections are required.

Resolution

The connection details and thermistor types are shown below;

To review the complete datasheet please click HERE.