Issue
Attempting to link from one I/A Series G3 station to another using a pop-up link and getting an error when using the browser. The error indicates - javax.baja.license.FeatureNotLicensedException: tridium:brand.
Environment
I/A Series G3 (all versions)
Cause
Created a PxFile with a bound label pop-up binding to open another link outside the station environment (e.g. history). The link works properly when using and viewing in Workbench but does not work with IE browser.
Resolution
The pop-up link through the browser currently does not support links to another station (supports only links within the same station). Recommend the graphic be located with the associated history in the same station if pop-up link required.