Issue
For various reasons it may be necessary to temporarily stop a schedule from driving its occupancy point, is there an easy way to accomplish this?
Environment
CyberStation
All CXs
All i2s
All b3s
Cause
Documentation
Resolution
If the schedule object is a Continuum schedule...
1. Edit the schedule object
2. Go to the 'Configuration' tab
3. Set the state to disabled.
For a BACnet schedule...
1. Edit the schedule object.
2. Go to the 'Current State' tab
3 Check the 'Out of service' box
To return control to the schedule re-enable it/put it back in service.