Issue
Licencing error in RAM log
Environment
Sigma
RAM
Micronet
Vista
Cause
The following error is seen in the RAM log when Sigma is installed.
Resolution
In Sigma, RAM licensing is done using the Sigma dongle.
In the "Remote Alarm Manager Computer Configuration Wizard"
Select: Start > Licence Scheme and ensure that the "Legacy Licence Schemes" is checked.