Which release of Microsoft Visio to use with StruxureWare Building Operation WorkPlace Tech Editor.

Issue

  • Which release of Microsoft Visio to use with StruxureWare Building Operation WorkPlace Tech Editor.
  • The following error context is encountered when trying to run WorkPlace Tech Editor to edit a program:


    WorkPlace Tech Editor returned errorClass not registered 0x80040154 REGDB_E_CLASSNOTREG 

Product Line

TAC I/A Series, SmartStruxure Solution

Environment

I/A Series LON controllers

WorkPlace Tech Editor.

Cause

A 64-bit version of Microsoft Visio 2010 can not be installed. Currently, only 32-bit versions of Microsoft Visio is supported for WorkPlace Tech

Resolution

The StruxureWare Building Operation - WorkPlace Tech Editor can use Visio 2010 SP1, Visio 2007 SP2, or Visio 2003 SP3, 32 bit versions only.