Issue
Xenta 700 restarts when updating a Menta Time Schedule using a Central Time Schedule in TAC Vista Workstation.
Environment
Xenta 701
Xenta 711
Xenta 721
Xenta 721
Cause
This issue is caused by a bug in the Xenta Server firmware.
Resolution
This bug has been fixed in the Xenta 700 5.1.7-SP1 firmware, available for download from the Exchange Extranet