Issue
Data not showing up in the consumption report.
Product Line
TAC I/NET
Environment
All versions of I/Net.
Cause
The points that are trending data are not matching up with the new host, therefore it is not collecting any data.
Resolution
After restoring the database, open up the trends editor and create or match the trends on the new Host PC.