Objects with a . character at the end of the object name will not bind to other objects.

Issue

Cannot bind an input with the name Intern.Temp.

Product Line

SmartStruxure Solution

Environment

  • StruxureWare Building Operation
  • Binding
  • Point Naming

Cause

While a "." may be used as a separating character within a point name, it is an illegal object name character when it appears as the last character.

StruxureWare Building Operation will generate an Illegal Character error when you attempt to name an object with a trailing "." character.

Resolution

Rename the object without a "." at the end of the name string and rebind it to the object.