SHD100: Using 24V AC power supply and 4-20mA output signal

Issue

The data sheet only lists AC power supply as an option when using the 0-10V output signal

Product Line

Field Devices

Environment

SHD100 006902320

SHD100-T 006902330

Cause

Sensor configuration options.

Resolution

For a transmitter the operating (normal) current is at once the measuring signal. If a rectified output is requested this means that DC voltage as supply voltage is required.