When tunnel through a UNC using an HTTP port other than 80 the Ax Serial Tunnel will not connect and locks up.

Issue

When tunnel through a UNC using an HTTP port other than 80 the Ax Serial Tunnel will not connect and locks up.

Product Line

TAC I/A Series

Environment

R2, G3 I/A Series tunneling

Cause

Including the port number after the IP address when entering the Host address in the Ax serial tunnel window will cause it to lock up trying to connect with the port entered.

Resolution

Do not include the port number after the IP address when entering the Host address in the Ax serial tunnel window.