Issue
Can Pelco's Control Point Software run on the same PC as I/NET Seven Software?
Product Line
Pelco, TAC INET
Environment
- All Windows OS
- I/NET Seven Software
- Pelco Control Point Software
Cause
The two software packages are not compatible with each other.
Resolution
Pelco's client software cannot be installed on the same PC that is running TAC I/NET Seven.
See TCON 301 - Chapter 6.