What is the factory default IP address for a new I/A Series G3 JACE-6 or JACE-7?

Issue

What is the factory default IP address for a new I/A Series G3 JACE-6 or JACE-7?

Product Line

TAC I/A Series

Environment

I/A Series G3, JACE-6 and JACE-7

Cause

Initial powerup and connection to Workbench

Resolution

Two female 10/100-Mbit Ethernet connections are provided on the JACE-6 and JACE-7 hardware platforms. These are RJ-45 connectors labeled LAN2 and LAN1.  Use a standard Ethernet patch cable for connecting to a hub or Ethernet switch. An activity LED for each Ethernet port is visible, and are labeled “LAN2” and “LAN1” on the cover.

The factory-default IP address for LAN1 on the JACE-6 and JACE-7 is 192.168.1.12n, where the last numeral n in the address matches the last digit of the JACE's serial number, and subnet mask is 255.255.255.0.  By default, LAN2 on the JACE-6 and JACE-7 is disabled.

The factory default platform username and password is tridium / niagara.