Issue
An object’s override and set pop-up boxes do not fully open in Niagara G3. You have to grab and pull the corner of the pop-up to open it completely. Niagara version 3.5.x is installed on a Windows 7 PC.
Environment
Niagara G3 Version 3.5.x and older
Cause
Versions of WorkBench prior to 3.6.31 have not been officially certified with Windows 7.
Resolution
The issue is more of a nuisance, but does not affect functionality in any way.
There are a couple of options you can try to try and correct the issue.
The first option is to try to reduce the font size in Windows 7.
- Click on the Start button and open the Control Panel
- Open the Fonts folder and select Change font size.
- Select smaller fro the font size and click apply
The other option is to change the screen resolution slightly.
Note: Since Niagara versions prior to 3.6.31 have not been certified for the Windows 7 operating environment, the above my not correct the issue.