Issue
Can't display values from a Modbus IP device where it is using a data type of swapped Longint (32 bit).
Environment
Continuum
Modbus IP XDriver (2nd Generation) v2.00012 and below
CX9680
ACX5720, ACX5740
bCX1-9640, bCX1-4040
PM9C Power Meter
Cause
Modbus IP Xdriver did not support the swapped Longint (32 bit) data type.
Resolution
Support for this data type was added to the Modbus IP XDriver (2nd Generation) in v2.00018 which is available on The Exchange Download Center at the link below: