The panes in webstation are empty and login happens without specifying a user or password.

Issue

The panes in Webstation are empty and login happens without specifying a user or password. When specifying the URL to webstation the user is automatically logged in to webstation but there are no objects in the panes.

Product Line

TAC Vista

Environment

TAC Vista Webstation 5.1.6/7

Cause

This is caused by using the wrong application pool in Internet Information Services (IIS) manager.

Resolution

Ensure that the application pool SE ASP.NET v4.0 Classic is used.

More information on how to set this and check other settings for Webstation can be found in the Lessons Learned Lessons Learned Article #4765.