Issue
Vista server crashes several times every day. Error message written in Windows event viewer:
Faulting application Tacos.exe, version 5.1.7.219, faulting module Tacdbi.dll, version 5.1.7.219, fault address 0x00075799.
Environment
TAC Vista 5.1.7
Cause
When doing a backup and the option "Retrieve trendlog data" is marked Vista will do a search for all trendlogs in the server and then go out and retrieve the logdata. Vista crash when the search for the trendlogs is made.
Resolution
In the backup object unmark the "Retrieve trendlog data" option.