Changing the Priority of System Alarms in StruxureWare Building Operation

Issue

How to change the priority of system generated alarms in StruxureWare Building Operation.

Product Line

SmartStruxure Solution

Environment

StruxureWare AS-L, AS-B, Enterprise Server (all versions)

Cause

no cause

Resolution

Currently, it is not possible to change the priority of system alarms. The default is value 100.  There are currently no plans to add the feature.