Microsoft Visual Studio causes Just-In-Time Debugging

Issue

Microsoft Visual Studio causes Just-In-Time Debugging

Product Line

Other

Environment

Windows Operating System

Cause

Visual Studio is installed on the PC and when attempting to perform a task, an error appears claiming Just-In-Time Debugging. 

Resolution

To disable Just-In-Time debugging:

  1. On the Tools menu, click Options.
  2. In the Options dialog box, select the Debugging folder.
  3. In the Debugging folder, select the Just-In-Time page.
  4. In the Enable Just-In-Time debugging of these types of code box, select or clear the relevant program types: Managed, Native, or Script.
  5. To disable Just-In-Time debugging, once it has been enabled, you must be running with Administrator privileges. Enabling Just-In-Time debugging sets a registry key, and Administrator privileges are required to change that key.
  6. Click OK.