Issue
When editing a card layout in EPI Designer how are the live fields linked to the Personnel attributes?
Environment
Cyberstation with card badging -B Option.
Cause
Clarification on how to link to personnel attributes
Resolution
- Select the "Dynamic Image" icon from the top menu, then use the cursor to draw a box the size of the photo required on the card.
- Right Click the new box and select "Properties"
- Select the Image Tab, then from the image type drop down select from Photograph, Signature or Fingerprint. In this case these 3 options do not require a Field Name entering as they already define the attribute required. Other settings can be selected / adjusted as required on the other tabs.
- Save the badge layout, close EPI Designer, then select File, Print Preview Card from the Make/Edit Badge screen. This will show how the Photo, Signature or Fingerprint image will look on the card.