Issue
Spare parts availability for Controlli MVL56 (Forta M700)
Environment
Controlli MVL56
Forta M700
Cause
Replacement parts
Resolution
Due to the spring return design of this actuator, no spare parts are available, with the possible exception of the PCBA. Any repairs should be done by the factory for safety reasons. However, MVL56 is a Controlli product and they should be contacted directly for further details.
If the M700 fails after the warranty then a new actuator is required, the MG900 SR is a lower cost alternative to the M700.