Clean db for Enterprise Server

Issue

How does one get a clean database for the Enterprise Server?

Product Line

SmartStruxure Solution

Environment

StruxureWare Buildings Operation site with Enterprise Server ES.

Cause

Need for clean database either for testing or start from scratch. 

Resolution

1. Stop the Enterprise Server using the StruxureWare Software Administrator

2. Then go to the location of your database using Windows Explorer. For this example it is C:\Documents and Settings\All Users\Application Data\Schneider Electric\StruxureWare 1.x\Enterprise Server

3. Rename the db and db_backup folder.

4. Reinstall the Enterprise Server portion of StruxureWare which will create a new db and db_backup folder with a clean database.

Note: Restoring a different database over the current database does not require the clean database state. Using the backup and restore procedure allows you to switch databases.