Issue
Door configured not to send forced entries access event but forced open alarms keep coming in the alarm viewer
Environment
CyberStation
CX9900
CX9702
CX9680
ACX5740
ACX5720
ACX7xxx
Cause
The filtering options in the door only filter out the access events, to stop the alarm from triggering modify the expression alarm algorithm.
Resolution
To have the doors send forced open alarms ONLY when configured to send the forced entry access event modify the expression in the Door Forced Open alarm enrollment as follows:
ForcedEntry = True and RecordValHist = True