Can the S-x96-PSU replace a PSU card in a UNC196 or 296 Controller with separate communication and processor cards?

Issue

Can the S-x96-PSU replace a PSU card in a UNC196 or 296 Controller with separate communication and processor cards?

Product Line

Satchwell Sigma

Environment

  • BAS
  • Sigma
  • S-x96-PSU
  • V53
  • 196
  • 296
  • UNC196
  • UNC296

Cause

Can the S-x96-PSU replace a PSU card in a UNC196 or 296 Controller with separate communication and processor cards?

Resolution

The S-x96-PSU can only be used with V53 type processor boards in BAS. Download the PIB here.

For BAS2800+, the separate comms and processor boards will need to be replaced with the V53 version.

****Note 1: For BAS2800+ V53 processor boards are only available till stocks are exhausted, and the upgrade path is to Sigma****

****Note 2: For BAS2000 and BAS2800, the upgrade path is to Sigma****