Issue
Are the Niagara G3 ENC-520-2 or the ENC-410-1 certified under UL-864?
Environment
Niagara G3
Cause
Product is being considered as a replacement for the Network 8000 GCM-86000 (which is UL-864 rated).
Resolution
Both the ENC-520-2 and ENC-410-1 are NOT fire-rated (or UL-864 approved).